Other topics about Operation Basics
The echo window, which appears in the lower part of the E5071C measurement screen, can be used to display a message or the return value (data) of an object.
You can use the COM objects listed below to enter values output to the echo window.
You can use the COM objects listed below to open the echo window.
Alternatively, you can also open the echo window using the following key sequence:
Macro Setup > Echo Window (ON)
You can use the COM object shown below to clear values output from the echo window.
Alternatively, you can also clear values output from the echo window using the following key sequence:
Macro Setup > Clear Echo