You can operate the E5071C using one of three operating methods: using keys on the front panel, using a mouse and keyboard, and using the touch screen. This section illustrates these three operating methods through the example in which the channel window layout is set to the four-channel display as shown in the following figure.
In the next section and those following it, a series of operations is expressed as follows:
Display > Allocate Traces > ![]()
Four-Trace Display

Press the DISPLAY key in the RESPONSE Block.

Press
or
key to move the cursor to the Allocate Traces, then press Enter or (
) key.

Press
or
key to move the cursor to
, then press Enter key.
From the Response menu, press Display key.

Click Allocate Traces.
Click ![]()
Press Display key after presetting the E5071C (Executing Preset key).

Click/Press Allocate Traces.
Click/Press any desired setting.