Other topics about Using Windows
The E5071C has the built-in clock that keeps track of the date and time. This clock is used for the following functions.
To display the current date and time in the instrument status bar at the lower part of the screen
To write date and time information when saving internal data or a VBA program
The Date & Time of E5071C clock can be changed by double-clicking the clock on the bottom right of the taskbar.
Below are the options to change the Date & Time of E5071C:
Double-click the clock at the bottom right of the taskbar. Click on the Change date and time settings. The Date and Time dialog box appears. Click on the Change date and time settings button. Perform the desired changes.
System > Misc Setup > Clock Setup > Set Date and Time....Similar to the earlier option, the Date and Time dialog box appears. Click on the Change date and time button. Perform the desired changes.
For windows 7/10, the administrator password is required to change the time and date setting when login as standard user.