Softkey display

Function

2-1(S21 S11)

Measure between test ports 1 and 2. selecting port 1 as the output.

3-1(S31 S11)

Measure between test ports 1 and 3. selecting port 1 as the output.

4-1(S41 S11)

Measure between test ports 1 and 4. selecting port 1 as the output.

1-2(S12 S22)

Measure between test ports 2 and 1. selecting port 2 as the output.

3-2(S32 S22)

Measure between test ports 2 and 3. selecting port 2 as the output.

4-2(S42 S22)

Measure between test ports 2 and 4. selecting port 2 as the output.

1-3(S13 S33)

Measure between test ports 3 and 1. selecting port 3 as the output.

2-3(S23 S33)

Measure between test ports 3 and 2. selecting port 3 as the output.

4-3(S43 S33)

Measure between test ports 3 and 4. selecting port 3 as the output.

1-4(S14 S44)

Measure between test ports 4 and 1. selecting port 4 as the output.

2-4(S24 S44)

Measure between test ports 4 and 2. selecting port 4 as the output.

3-4(S34 S44)

Measure between test ports 4 and 3. selecting port 4 as the output.