Selecting Calibration Kit

Other topics about Basic Calibration

Overview

Before executing calibration, you need to select a calibration kit.

If you use a calibration kit other than a predefined one, you need to define it. If the connector type of the standard of the calibration kit you use has polarity (the distinction between male and female), you need to change the standard class definition of the calibration kit depending on the standard you actually use. For more information, see Modifying Calibration Kit Definition.

Procedure

  1. Press Channel Next/Channel Prev to select the channel for which you want to select the calibration kit.

  2. Press Cal.

  3. Click Cal Kit, then select the calibration kit.

  4.  If the name (label) of the calibration kit has been changed, the label is displayed as the softkey.

  5.  An asterisk (*) on the upper right of the softkey corresponding to a predefined calibration kit indicates that its definition value has been changed from the factory setting, by the user.