Performing Parameter Conversion of Measurement Results

Other topics about Data Analysis

Overview

You can use the parameter conversion function to convert the measurement results of the S-Parameter (Sab) to the following parameters.

where:

Z0a: Characteristic impedance of port a

Z0b: Characteristic impedance of port b

When the fixture simulator function is turned ON and the port impedance function is ON, the value set in the port impedance conversion is used. In other cases, the system Z0 (preset value: 50 Ω) is used.

Procedure

ON/OFF

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to activate a trace at which you want to use the marker.

  2. Press Analysis.

  3. Click Conversion > Conversion to turn ON the conversion function.

Selecting Conversion Target Parameter

  1. Press Channel Next/Channel Prev and Trace Next/Trace Prev to activate a trace at which you want to use the marker.

  2. Press Analysis.

  3. Click Conversion > Function.

  4. Click the softkey corresponding to the parameter to which you want to convert the result.

When the conversion function is ON, the selected parameter is displayed in the Trace Status Area.