Other topics about Data Output
Along with printing, the E5072A allows the user to save screen images as Bitmap (.bmp) or Portable Network Graphics (.png) files. Saved files can be loaded into PC application software for further processing.
Follow the procedure below to save a screen image to a file.
Display the screen to be saved as a file. If you want to save the screen with a white background, set the display mode to inverted display before saving the screen. For details about display mode, see Setting Display Colors.
Press System. The screen image at the time System key is pressed is the image that will be saved.
Press Dump Screen Image... to open the Save As dialog box. "24-bit Bitmap (*.bmp)" or "Portable Network Graphics (*.png)" can be selected as the file type.
Select the destination folder and type a file name.
Press Save to save the screen image of E5072A to a file.