Measuring Parameters with Cable

Other Measurement Examples

Overview

This section introduces an example of how to detect the location of a mismatch that occurs in a cable by using the time domain function.

Procedure

In this example, a DUT is evaluated according to the steps.

Step

Description

1. Setting the Measurement Conditions

Set the measurement conditions.

2. Executing Calibration

Execute calibration.

3. Connecting the DUT

Connect the DUT.

4. Auto Scale

Execute auto scale.

5. Setting the Time Domain Function

Set the time domain function.

1. Setting the Measurement Conditions

Follow these steps to set the measurement conditions:

Setting Description

Key Operation

Presetting

Preset > OK

Stop frequency: 3 GHz

Stop > 3 > G/n 

Number of points: 201

Sweep Setup > Points > 2 > 0 > 1 > x1

Specifying the low-pass mode sweep condition

Analysis > Transform > Set Freq Low Pass

Measurement parameter: S11

Meas > S11

2. Executing Calibration

By following 1-Port Calibration (reflection test), execute 1-port calibration on port 1.

 

3. Connecting the DUT

Connect the DUT as shown below.

4. Auto Scale

Execute the auto scale function.

Setting Description

Key Operation

Executing auto scale

Scale > Auto Scale

 

5. Setting the Time Domain Function

Set the conversion function to display the response in the time domain. If you enable this setting, the response in time domain is displayed as shown figure below. A peak indicating a small mismatch appears at the location of the connector.

Setting Description

Key Operation

Data format: real

Format > Real

Setting the transformation type to low-pass impulse

Analysis > Transform > Type > Lowpass Imp

Setting the window type to maximum.

Analysis > Transform > Window > Maximum

Setting the display range: from 0 s to 20 ns

Analysis > Transform > Start > 0 > x1

Analysis > Transform > Stop > 2 > 0 > G/n

Enabling the transformation function

Analysis > Transform > Transform > ON

Executing auto scale

Scale > Auto Scale