Method (Write-only)
Parse(Scpi)
Return = Parse(Scpi?)
Executes an SCPI command of the E5072A.
The Parse object is a little slower in the execution speed than the COM object which has the same function as the SCPI command because it must parse the message string of the SCPI command.
|
Parameter |
Scpi |
|
Description |
SCPI command |
|
Data type |
Character string type (String) |
|
Parameter |
Return |
|
Description |
Response (query) of the SCPI command |
|
Data type |
Character string type (String) |
Dim Start As String
Parse(":SENS1:FREQ:STAR 100E6")
Start = Parse(":SENS1:FREQ:STAR?")
Dim TtlLbl As String
Parse(":DISP:WIND1:TITL:DATA ""filter""")
TtlLbl = Parse(":DISP:WIND1:TITL:DATA?")
Dim Fmt As String
Parse(":CALC1:PAR2:SEL")
Parse(":CALC1:FORM SMIT")
Fmt = Parse(":CALC1:FORM?")
Dim BckLght As String
Parse(":SYST:BACK OFF")
BckLght = Parse(":SYST:BACK?")
No equivalent key is available on the front panel.