SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BALanced.DEFine(Name)

Object type

Property (Read-Write)

Syntax

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BALanced.DEFine(Name) = Param

Param = SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BALanced.DEFine(Name)

Description

This command sets/gets the measurement parameter when the balance device type is "balance", for the selected trace of the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command.

Variable

Parameter

Name

Description

Trace Name

Data type

Character string type (String)

 

Parameter

Param

Description

Measurement parameter

Data type

Character string type (String)

Range

Select from the following.

  • "SDD11": Specifies Sdd11.

  • "SCD11": Specifies Scd11.

  • "SDC11": Specifies Sdc11.

  • "SCC11": Specifies Scc11.

Preset value

"SDD11"

Examples

Dim BalPara As String
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bal"

SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"
SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.BALanced.DEFine("duptrace") = "sdd11"
BalPara = SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.BALanced.DEFine("duptrace")

Related objects

SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice

Equivalent key

Analysis > Fixture Simulator|[Meas] > Sdd11|Scd11|Sdc11|Scc11

Equivalent SCPI command

Syntax

:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:BALanced[:DEFine] <string>, {SDD11|SCD11|SDC11|SCC11}

:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:BALanced[:DEFine]? <string>

 Query response

{SDD11|SCD11|SDC11|SCC11}<newline><^END>

Example of use

10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""

20 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:BAL ""DUPTRACE"",SDD21"
30 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:BAL? ""DUPTRACE"""
40 ENTER 717;A$