SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BBALanced.DEFine(Name)

Object type

Property (Read-Write)

Syntax

SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BBALanced.DEFine(Name) = Param

Param = SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.BBALanced.DEFine(Name)

Description

This command sets/gets the measurement parameter when the balance device type is "balance-balance", for the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command. This function is available in the revision A.9.60 and above.

Variable

Parameter

Name

Description

Trace Name

Data type

Character string type (String)

 

Parameter

Param

Description

Measurement parameter

Data type

Character string type (String)

Range

Select from the following.

  • "SDD11": Specifies Sdd11.

  • "SDD21": Specifies Sdd21.

  • "SDD12": Specifies Sdd12.

  • "SDD22": Specifies Sdd22.

  • "SCD11": Specifies Scd11.

  • "SCD21": Specifies Scd21.

  • "SCD12": Specifies Scd12.

  • "SCD22": Specifies Scd22.

  • "SDC11": Specifies Sdc11.

  • "SDC21": Specifies Sdc21.

  • "SDC12": Specifies Sdc12.

  • "SDC22": Specifies Sdc22.

  • "SCC11": Specifies Scc11.

  • "SCC21": Specifies Scc21.

  • "SCC12": Specifies Scc12.

  • "SCC22": Specifies Scc22.

  • "IMB1":Specifies Imbalance1.

  • "IMB2":Specifies Imbalance2.

  • "CMRR": Specifies CMRR (Sdd21/Scc21).

Preset value

"SDD11"

Examples

Dim BbalPara As String
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "bbal"
SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"

SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.BBALanced.DEFine("duptrace") = "sdd21"
BbalPara = SCPI.CALCulate(1).FSIMulator.BALun.PARameter.BBALanced.DEFine("duptrace")

Related objects

SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice

Equivalent key

Analysis > Fixture Simulator|[Meas] > Sdd11|Sdd21|Sdd12|Sdd22|Scd11| Scd21|Scd12|Scd22|Sdc11| Sdc21|Sdc12|Sdc22|Scc11|Scc21|Scc12|Scc22| Imbalance1|Imbalance2|Sdd21/Scc21

Equivalent SCPI command

Syntax

:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:BBALanced[:DEFine] <string>, {SDD11|SDD21|SDD12|SDD22|SCD11|SCD21|SCD12|SCD22|SDC11|SDC21|SDC12|SDC22|SCC11|
SCC21|SCC12|SCC22|IMB1|IMB2| CMRR}

:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:BBALanced[:DEFine]? <string>

Query response

{SDD11|SDD21|SDD12|SDD22|SCD11|SCD21|SCD12|SCD22|SDC11|SDC21|SDC12|SDC22|
SCC11|SCC21|SCC12|SCC22|IMB1|IMB2|CMRR}<newline><^END>

Example of use

10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""

20 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:BBAL ""DUPTRACE"",SDD21"
30 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:BBAL? ""DUPTRACE"""
40 ENTER 717;A$