Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.SSBalanced.DEFine(Name) = Param
Param = SCPI.CALCulate(Ch).FSIMulator.BALun.PARameter.TNAMe.SSBalanced.DEFine(Name)
This command sets/gets the measurement parameter when the balance device type is "unbalance-unbalance-balance", for the selected trace of the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command. This function is available in the revision A.9.60 and above.
Parameter |
Name |
Description |
Trace Name |
Data type |
Character string type (String) |
Parameter |
Param |
Description |
Measurement parameter |
Data type |
Character string type (String) |
Range |
Select from the following.
|
Preset value |
"SSS11" |
Dim SsbPara As String
SCPI.CALCulate(1).FSIMulator.BALun.DEVice = "ssb"
SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"
SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.SSBalanced.DEFine("duptrace") = "sds31"
SsbPara = SCPI.CALCulate(1).FSIMulator.BALun.PARameter.TNAMe.SSBalanced.DEFine("duptrace")
SCPI.CALCulate(Ch).FSIMulator.BALun.DEVice
Analysis > Fixture Simulator|[Meas] > Sss11|Sss21|Sss12|Sss22|Sds31| Sds32|Ssd13|Ssd23|Scs31|Scs32|Ssc13|Ssc23|Sdd33|Scd33|Sdc33|Scc33| Imbalance1|Imbalance2|Imbalance3|Imbalance4|Sds31/Scs31|Sds32/Scs32
:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:SSBalanced[:DEFine] <string>, {SSS11|SSS21|SSS12|SSS22|SDS31|SDS32|SSD13|SSD23|SCS31|SCS32|SSC13|SSC23|SDD33|SCD33|
SDC33|SCC33|IMB1|IMB2|IMB3|IMB4|CMRR1|CMRR2}
:CALCulate{[1]-160}:FSIMulator:BALun:PARameter:TNAMe:SSBalanced[:DEFine]? <string>
{SSS11|SSS21|SSS12|SSS22|SDS31|SDS32|SSD13|SSD23|SCS31|SCS32|SSC13|SSC23|SDD33|SCD33|SDC33|SCC33|IMB1|IMB2|IMB3|IMB4|CMRR1|CMRR2}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""
20 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:SSB ""DUPTRACE"",SDS31"
30 OUTPUT 717;":CALC1:FSIM:BAL:PAR:TNAM:SSB? ""DUPTRACE"""
40 ENTER 717;A$