Property (Read-Write)
SCPI.CALCulate(Ch).PARameter.TNAMe.DEFine(Name) = Param
Param = SCPI.CALCulate(Ch).PARameter.TNAMe.DEFine(Name)
This command sets/gets the measurement parameter of the selected trace for the selected channel (Ch). The trace can be selected by the trace name once its defined earlier with SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA command.
Parameter |
Name |
Description |
Trace Name |
Data type |
Character string type (String) |
Parameter |
Param |
Description |
Measurement parameter |
Data type |
Character string type (String) |
Range |
Select either one of the following:
|
Preset value |
"S11" |
Dim MeasPara As String
SCPI.CALCulate(1).PARameter(1).TNAMe.DATA = "duptrace"
SCPI.CALCulate(1).PARameter.TNAMe.DEFine("duptrace") = "S21"
MeasPara = SCPI.CALCulate(1).PARameter.TNAMe.DEFine("duptrace")
SCPI.CALCulate(Ch).PARameter(Tr).TNAMe.DATA
SCPI.CALCulate(Ch).PARameter.TNAME.SELect
SCPI.CALCulate(Ch).PARameter.TNAME.SPORt
Meas > S<XY> {X=1-2;Y=1-2}|
Meas > Absolute > R<X> {X=1-2}|A|B
Meas > Aux Input 1|Aux Input 2
:CALCulate{[1]-160}:PARameter:TNAMe:DEFine <string>, {S11|S21|S12|S22|A|B|R1|R2|Aux1|AUX2}
:CALCulate{[1]-160}:PARameter:TNAMe:DEFine? <string>
{S11|S21|S12|S22|A|B|R1|R2|Aux1|AUX2}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:TNAM:DATA ""DUPTRACE"""
20 OUTPUT 717;":CALC1:PAR:TNAM:DEF ""DUPTRACE"", S21"
30 OUTPUT 717;":CALC1:PAR:TNAM:DEF? ""DUPTRACE"""
40 ENTER 717;A$