Property (Read-Write)
SCPI.CALCulate(Ch).SELected.EQUation.TEXT = Data
Data = SCPI.CALCulate(Ch).SELected.EQUation.TEXT
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).EQUation.TEXT = Data
Data = SCPI.CALCulate(Ch).TRACe(Tr).EQUation.TEXT
This command sets/gets the equation in the Equation Editor. For valid parameters that can be used in this equation, refer to the Equation Editor.
Optionally, you can select the trace and set/get the equation in the Equation Editor for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Ch |
|
Description |
Channel Number |
|
Range |
1 to 36 |
|
Parameter |
Data |
|
Description |
Sets/Gets the equation in the Equation Editor |
|
Data type |
Character string type (String) |
Dim strEq As String
SCPI.CALCulate(1).SELected.EQUation.TEXT = “Example=S21/(1-S11)”
strEq = SCPI.CALCulate(1).SELected.EQUation.TEXT
SCPI.CALCulate(Ch).SELected.EQUation.STATE
SCPI.CALCulate(Ch).SELected.EQUation.VALid
No equivalent key is available on the front panel for Equation Text but Equation Editor can be accessed through Display > Equation Editor.
:CALCulate{[1]-160}[:SELected]:EQUation:TEXT <string1>
:CALCulate{[1]-160}[:SELected]:EQUation:TEXT?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:EQUation:TEXT <string1>
:CALCulate{[1]-160}:TRACe{[1]-16}:EQUation:TEXT?
<string 1><^END>
10 OUTPUT 717;":CALC1:SELected:EQUation:TEXT?"
30 ENTER 717;A$