Property (Read-Write)
SCPI.CALCulate(Ch).FSIMulator.BALun.DZConversion.STATe = Status
Status = SCPI.CALCulate(Ch).FSIMulator.BALun.DZConversion.STATe
This command turns ON/OFF the differential port impedance conversion function when the fixture simulator function is ON, for all the balance ports of selected channel (Ch).
Parameter |
Status |
Description |
ON/OFF of the differential port impedance conversion function |
Data type |
Boolean type (Boolean) |
Range |
Select from the following.
|
Preset value |
False or OFF |
Dim DifZcon As Boolean
SCPI.CALCulate(1).FSIMulator.BALun.DZConversion.STATe = True
DifZcon = SCPI.CALCulate(1).FSIMulator.BALun.DZConversion.STATe
SCPI.CALCulate(Ch).FSIMulator.BALun.DZConversion.BPORt(Bpt).IMAGinary
SCPI.CALCulate(Ch).FSIMulator.BALun.DZConversion.BPORt(Bpt).REAL
SCPI.CALCulate(Ch).FSIMulator.BALun.DZConversion.BPORt(Bpt).Z0.R
SCPI.CALCulate(Ch).FSIMulator.STATe
Analysis > Fixture Simulator > Diff ZConversion > Diff ZConversion
:CALCulate{[1]-160}:FSIMulator:BALun:DZConversion:STATe {ON|OFF|1|0}
:CALCulate{[1]-160}:FSIMulator:BALun:DZConversion:STATe?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:FSIM:BAL:DZC:STAT ON"
20 OUTPUT 717;":CALC1:FSIM:BAL:DZC:STAT?"
30 ENTER 717;A