Property (Read-Write)
SCPI.CALCulate(Ch).PARameter(Tr).DEFine = Param
Param = SCPI.CALCulate(Ch).PARameter(Tr).DEFine
This command sets/gets the measurement parameter of the selected trace (Tr), for the selected channel (Ch).
Parameter |
Param |
Description |
Measurement parameter |
Data type |
Character string type (String) |
Range |
Select either one of the following:
|
Preset value |
"S11" |
Dim MeasPara As String
SCPI.CALCulate(1).PARameter(1).DEFine = "s21"
MeasPara = SCPI.CALCulate(1).PARameter(1).DEFine
Meas > S<XY> {X=1-2;Y=1-2}|
Meas > Absolute > R<X> {X=1-2}|A|B
Meas > Aux Input 1|Aux Input 2
:CALCulate{[1]-160}:PARameter{[1]-16}:DEFine <string>{S11|S21|S12|S22|A|B|R1|R2|Aux1|AUX2}
:CALCulate{[1]-160}:PARameter{[1]|-16}:DEFine?
{S11|S21|S12|S22|A|B|R1|R2|Aux1|AUX2}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:DEF S21"
20 OUTPUT 717;":CALC1:PAR1:DEF?"
30 ENTER 717;A$