Method (Write-only)
SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).FUNCtion.EXECute
This command executes the analysis specified with the SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE object, for the active trace of selected channel (Ch).
Optionally, you can select the trace and execute the analysis specified with the SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE object for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.EXECute
SCPI.CALCulate(Ch).SELected.FUNCtion.DATA
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE
SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STATe
No equivalent key is available on the front panel.
:CALCulate{[1]-160}[:SELected]:FUNCtion:EXECute
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:FUNCtion:EXECute
10 OUTPUT 717;":CALC1:FUNC:EXEC"