SCPI.CALCulate(Ch).SELected.LIMit.REPort.DATA

Object type

Property (Read Only)

Syntax

Data = SCPI.CALCulate(Ch).SELected.LIMit.REPort.DATA

 

The following syntax is also supported:

Data = SCPI.CALCulate(Ch).TRACe(Tr).LIMit.REPort.DATA

Description

This command reads the stimulus values (frequency, power level or time) at all the measurement points that failed the limit test, for the active trace of selected channel (Ch).

 

Optionally, you can select the trace and read the stimulus values at all the measurement points that failed the limit test, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.

Variable

Parameter

Data

Description

Indicates the array data for failed measurement points (can be read out with the SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts object).

Data type

Variant type (Variant)

Examples

Dim FailData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.LIMit.STATe = True
FailData = SCPI.CALCulate(1).SELected.LIMit.REPort.DATA

Related objects

SCPI.CALCulate(Ch).PARameter(Tr).SELect

SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts

SCPI.CALCulate(Ch).SELected.LIMit.STATe

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:CALCulate{[1]-160}[:SELected]:LIMit:REPort[:DATA]?

 

The following syntax is also supported:

:CALCulate{[1]-160}:TRACe{[1]-16}:LIMit:REPort[:DATA]?

Query response

{numeric 1},… ,{numeric N}<newline><^END>

Where N is the number of the measurement points that failed (can be read out with the :CALC{1-160}:LIM:REP:POIN? command).

Example of use

10 OUTPUT 717;":CALC1:LIM:REP:POIN?"
20 ENTER 717;A
30 REDIM B(1:A)
40 OUTPUT 717;":CALC1:LIM:REP?"
50 ENTER 717;B(*)