Property (Read-Write)
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.KBESsel = Value
Value = SCPI.CALCulate(Ch).SELected.TRANsform.TIME.KBESsel
The following syntax is also supported:
SCPI.CALCulate(Ch).TRACe(Tr).TRANsform.TIME.KBESsel = Value
Value = SCPI.CALCulate(Ch).TRACe(Tr).TRANsform.TIME.KBESsel
This command sets/gets the shape of the Kayser Bessel window used for the transformation function of the time domain function, for the active trace of selected channel (Ch).
Optionally, you can select the trace and set/get the shape of the Kayser Bessel window used for the transformation function of the time domain function, for the trace just by executing the above TRACe(Tr) command. You do not need to execute SCPI.CALCulate(Ch).PARameter(Tr).SELect.
|
Parameter |
Value |
|
Description |
The value of b |
|
Data type |
Double precision floating point type (Double) |
|
Range |
0 to13 |
|
Preset value |
6 |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Beta As Double
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.TRANsform.TIME.KBESsel = 3
Beta = SCPI.CALCulate(1).SELected.TRANsform.TIME.KBESsel
SCPI.CALCulate(Ch).SELected.TRANsform.TIME. IMPulse.WIDTh
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.STEP.RTIMe
SCPI.CALCulate(Ch).SELected.TRANsform.TIME.STATe
SCPI.CALCulate(Ch).PARameter(Tr).SELect
Analysis > Transform > Center
:CALCulate{[1]-160}[:SELected]:TRANsform:TIME:KBESsel <numeric>
:CALCulate{[1]-160}[:SELected]:TRANsform:TIME:KBESsel?
The following syntax is also supported:
:CALCulate{[1]-160}:TRACe{[1]-16}:TRANsform:TIME:KBESsel <numeric>
:CALCulate{[1]-160}:TRACe{[1]-16}:TRANsform:TIME:KBESsel?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:TRAN:TIME:KBES 3"
20 OUTPUT 717;":CALC1:TRAN:TIME:KBES?"
30 ENTER 717;A