SCPI.CONTrol.HANDler.E.DATA

Object type

Property (Read-Write)

Syntax

SCPI.CONTrol.HANDler.E.DATA = Value (for output)

Value = SCPI.CONTrol.HANDler.E.DATA (for input port)

Description

When input/output port E (port C + port D) of the handler I/O is set to the output port, outputs port information to output port E (C0 to D3).

When input/output port E of the handler I/O is set to the input port, reads out port information inputted to port E (C0 to D3).

Port information is output as 8-bit binary data using C0 as LSB and D3 as MSB.

Variable

Parameter

Value

Description

Port information (output/input)

Data type

Long integer type (Long)

Range

0 to 255

Note

If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set.

Examples

SCPI.CONTrol.HANDler.C.MODE = "outp"
SCPI.CONTrol.HANDler.D.MODE = "outp"
SCPI.CONTrol.HANDler.E.DATA = 128

Dim HdlEinp As Long
SCPI.CONTrol.HANDler.C.MODE = "inp"
SCPI.CONTrol.HANDler.D.MODE = "inp"
HdlEinp = SCPI.CONTrol.HANDler.E.DATA

Related objects

SCPI.CONTrol.HANDler.C.MODE

SCPI.CONTrol.HANDler.D.MODE

SCPI.CONTrol.HANDler.C.DATA

SCPI.CONTrol.HANDler.D.DATA

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:CONTrol:HANDler:E[:DATA] <numeric>

:CONTrol:HANDler:E[:DATA]?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":CONT:HAND:C:MODE OUTP"
20 OUTPUT 717;":CONT:HAND:D:MODE OUTP"
30 OUTPUT 717;":CONT:HAND:E 128"

10 OUTPUT 717;":CONT:HAND:C:MODE INP"
20 OUTPUT 717;":CONT:HAND:D:MODE INP"
30 OUTPUT 717;":CONT:HAND:E?"
40 ENTER 717;A