SCPI.DISPlay.UPDate.IMMediate

Object type

Method (Write-only)

Syntax

SCPI.DISPlay.UPDate.IMMediate

Description

This command executes the display update once when the display update of the LCD screen is set to OFF (specifying False with the SCPI.DISPlay.ENABle object),

Examples

SCPI.DISPlay.ENABle = False
SCPI.DISPlay.UPDate.IMMediate

Related objects

SCPI.DISPlay.ENABle

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:DISPlay:UPDate[:IMMediate]

Example of use

10 OUTPUT 717;":DISP:UPD"