Parameter
Ch
Description
Channel number
Data Type
Long integer type (Long)
Range
1 to 160
Preset Value
1
Note
If the specified variable is out of the allowable setup range, an error occurs when executed.