Parameter |
Ch |
Description |
Channel number |
Data Type |
Long integer type (Long) |
Range |
1 to 160 |
Preset Value |
1 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. Status Register for Limit/Bandwidth Limit/Ripple Limit Test is available up to 16 channel. |