Parameter |
Nwk |
Description |
Number of network |
Data type |
Long integer type (Long) |
Range |
1 to 4
1, 2 (4-port touchstone file only) 3 (6-port touchstone file only) 4 (8-port touchstone file only) |
Preset value |
1 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |