Property (Write Only)
SCPI.MMEMory.STORe.CHANnel.STATe = Register
This command saves the instrument state of the items set for the active channel specific to that channel only into the specified register (volatile memory).
Parameter |
Register |
Description |
Register |
Data type |
Character string type (String) |
Range |
Select from the following: "A": Specifies register A. "B": Specifies register B. "C": Specifies register C. "D": Specifies register D. |
Note |
If an instrument state has been saved already in the specified register, its contents are overwritten. |
SCPI.MMEMory.STORe.CHANnel.STATe = "a"
SCPI.MMEMory.LOAD.CHANnel.STATe
SCPI.DISPlay.WINDow(Ch).ACTivate
Save/Recall > Save Channel > A|B|C|D
:MMEMory:STORe:CHANnel[:STATe] {A|B|C|D}
10 OUTPUT 717;":MMEM:STOR:CHAN A"