Property (Write Only)
SCPI.MMEMory.STORe.STATe = File
This command saves the instrument state (contents to be saved specified with the SCPI.MMEMory.STORe.STYPe object) into a file with the .sta extension.
Specify the file name with the extension. When you use directory names and file name, separate them with "\ " (back slash), or "/" (slash).
Parameter |
File |
Description |
File name to save the instrument state (extension ".sta") |
Data type |
Character string type (String) |
Range |
254 characters or less |
Note |
If a file with the same name as the specified file name exists, its contents are overwritten. |
Dim StaType As String
SCPI.MMEMory.STORe.STYPe = "cdst"
SCPI.MMEMory.STORe.STATe = "d:\state01.sta"
Dim StaType As String
SCPI.MMEMory.STORe.STYPe = "cdst"
SCPI.MMEMory.STORe.STATe = "test/state01.sta"
Save/Recall > Save State
:MMEMory:STORe[:STATe] <string>
10 OUTPUT 717;":MMEM:STOR ""Test1/State01.sta"""
10 OUTPUT 717;":MMEM:STOR ""D:State01.sta"""