SCPI.SENSe(Ch).SEGMent.SLOCal.DATA

Object type

Property (Read-Write)

Syntax

SCPI.SENSe(Ch).SEGMent.SLOCal.DATA = Data

Data = SCPI.SENSe(Ch).SEGMent.SLOCal.DATA

Description

This command sets/gets the Shift LO state of each segment in the segment sweep table for the selected channel (Ch).

Variable

Parameter

Data

Description

Sets/gets the Shift LO state

Data type

Variant type array (Range)

Examples

Dim SegmData As Variant
Dim SegmSLocalData As Variant


SCPI.SENSe(1).SEGMent.DATA = Array(5,0,0,1,0,0,2, _
1E9,3E9,11,0,3E9,4E9,51,-10,4E9,6E9,11,10)
SegmData = SCPI.SENSe(1).SEGMent.DATA


SegmSLocalData = Array(1, 0, 0)
SCPI.SENSe(1).SEGMent.SLOCal.DATA = SegmSLocalData
SegmSLocalData = SCPI.SENSe(1).SEGMent.SLOCal.DATA

Related objects

SCPI.SENSe(Ch).SEGMent.SLOCal.STATe

SCPI.SENSe(Ch).SEGMent.DATA

Equivalent key

Sweep Setup > Edit Segment Table

Equivalent SCPI command

Syntax

 

:SENSe{[1]-160}:SEGMent:SLOCal:DATA <state 1>, <state 2>,..., <state N>

:SENSe{[1]-160}:SEGMent:SLOCal:DATA?

Where N is the number of segments.

Query Response

{numeric 1},...,{numeric N}<newline><^END>

Example of use

10 DIM H(1:3)
20 OUTPUT 717;":SENS1:SEGM:DATA 5,0,1,0,0,0,3,";
30 OUTPUT 717;"1E9,3E9,11,70e3,";
40 OUTPUT 717;"3E9,4E9,51,7e3,";
50 OUTPUT 717;"4E9,6E9,11,70e3"
60 OUTPUT 717;":SENS1:SEGM:SLOCal:DATA 1, 0, 0"
70 OUTPUT 717;":SENS1:SEGM:SLOCal:DATA?"
80 ENTER 717;H(*)