Property (Read-only)
Value = SCPI.SERVice.SWEep.POINts
This command reads the upper limit of the number of measurement points at the current configuration.
Parameter |
Value |
Description |
Upper limit of the number of points |
Data type |
Long integer type (Long) |
Dim MaxPoin As Long
MaxPoin = SCPI.SERVice.SWEep.POINts
No equivalent key is available on the front panel.
:SERVice:SWEep:POINts?
{numeric}<newline><^END>
10 OUTPUT 717;":SERV:SWE:POIN?"
20 ENTER 717;A