Property (Read-Write)
SCPI.SOURce(Ch).POWer.STOP = Value
Value = SCPI.SOURce(Ch).POWer.STOP
This command sets/gets the stop value of the sweep range for the power sweep for channels 1 to 160 (Ch).
Parameter |
Value |
Description |
Stop value |
Data type |
Double precision floating point type (Double) |
Range |
Varies depending on the power range: 30 kHz to 5 GHz –55 to 10 dBm 5 to 6 GHz –55 to 9 dBm 6 to 7 GHz –55 to 8 dBm 7 to 8.5 GHz –55 to 7 dBm |
Preset value |
0 |
Unit |
dBm |
Resolution |
0.05 |
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Pstop As Double
SCPI.SOURce(1).POWer.STOP = 10
Pstop = SCPI.SOURce(1).POWer.STOP
SCPI.SOURce(Ch).POWer.ATTenuation.DATA
Stop
:SOURce{[1]-160}:POWer:STOP <numeric>
:SOURce{[1]-160}:POWer:STOP?
{numeric}<newline><^END>
10 OUTPUT 717;":SOUR1:POW:STOP 10"
20 OUTPUT 717;":SOUR1:POW:STOP?"
30 ENTER 717;A