Property (Read-only)
Value = SCPI.STATus.QUEStionable.BLIMit.CHANnel(Ch).EVENt
This command reads the value of the "Questionable Bandwidth Limit Channel Status Event Register" of the specified channel.
Parameter |
Value |
Description |
The value of the Questionable Bandwidth Limit Channel Status Event Register |
Data type |
Long integer type (Long) |
For information on the variable (Ch), see Ch.
Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.BLIMit.CHANnel(1).EVENt
No equivalent key is available on the front panel.
:STATus:QUEStionable:BLIMit:CHANnel{[1]-160}[:EVENt]?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:BLIM:CHAN1?"
20 ENTER 717;A