Property (Read-only)
Value = SCPI.STATus.QUEStionable.BLIMit.ELIMit.EVENt
This command reads the value of the Questionable Bandwidth Limit Extra Status Event Register.
Parameter |
Value |
Description |
The value of the Questionable Bandwidth Limit Extra Status Event Register. |
Data type |
Long integer type (Long) |
Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.BLIMit.ELIMit.EVENt
No equivalent key is available on the front panel.
:STATus:QUEStionable:BLIMit:ELIMit[:EVENt]?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:BLIM:ELIM?"
20 ENTER 717;A