SCPI.STATus.QUEStionable.BLIMit.ENABle

Object type    

Property (Read-Write)

Syntax         

SCPI.STATus.QUEStionable.BLIMit.ENABle = Value

Value = SCPI.STATus.QUEStionable.BLIMit.ENABle

Description

This command sets/gets the value of the Questionable Bandwidth Limit Status Enable Register.

Variable

Parameter

Value

Description

The value of the Questionable Bandwidth Limit Status Enable Register.

Data type

Long integer type (Long)

Range

0 to 65535

Preset value

Varies depending on the upper limit setting of the number of channels/traces.

Note

Bits 15 cannot be set to 1.

Examples

Dim Stat As Long
SCPI.STATus.QUEStionable.BLIMit.ENABle = 16
Stat = SCPI.STATus.QUEStionable.BLIMit.ENABle

Related objects

SCPI.STATus.QUEStionable.ENABle

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:STATus:QUEStionable:BLIMit:ENABle <numeric>

:STATus:QUEStionable:BLIMit:ENABle?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":STAT:QUES:BLIM:ENAB 16"
20 OUTPUT 717;":STAT:QUES:BLIM:ENAB?"
30 ENTER 717;A