Property (Read-only)
Value = SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).CONDition
This command reads the value of the Questionable Limit Channel Extra Status Condition Register of the specified channel (Ch).
Parameter |
Value |
Description |
Value of the Questionable Limit Channel Extra Status Condition Register |
Data type |
Long integer type (Long) |
Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.LIMit.CHANnel(1).ECHannel.CONDition
SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).ECHannel.NTRansition
SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).ECHannel.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:LIMit:CHANnel{[1]-160}:ECHannel:CONDition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:LIM:CHAN1:ECH:COND?"
20 ENTER 717;A