Property (Read-Write)
SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).PTRansition = Value
Value = SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).PTRansition
This command sets/gets the value of the positive transition filter of the Questionable Limit Channel Status Register of the specified channel (Ch).
Parameter |
Value |
Description |
Value of the positive transition filter |
Data type |
Long integer type (Long) |
Range |
0 to 65535 |
Preset value |
Varies depending on the upper limit setting for the channel/trace number. |
Note |
The bit 15 can not be set to 1. |
Dim Stat As Long
SCPI.STATus.QUEStionable.LIMit.CHANnel(1).PTRansition = 0
Stat = SCPI.STATus.QUEStionable.LIMit.CHANnel(1).PTRansition
SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).EVENt
SCPI.STATus.QUEStionable.LIMit.CHANnel(Ch).NTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:LIMit:CHANnel{[1]-160}:PTRansition <numeric>
:STATus:QUEStionable:LIMit:CHANnel{[1]-160}:PTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:LIM:CHAN1:PTR 16"
20 OUTPUT 717;":STAT:QUES:LIM:CHAN1:PTR?"
30 ENTER 717;A