Property (Read-Write)
SCPI.STATus.QUEStionable.LIMit.ELIMit.NTRansition = Value
Value = SCPI.STATus.QUEStionable.LIMit.ELIMit.NTRansition
This command sets/gets the value of the negative transition filter of the Questionable Limit Extra Status Register.
Parameter |
Value |
Description |
Value of the negative transition filter |
Data type |
Long integer type (Long) |
Range |
0 to 65535 |
Preset value |
0 |
Note |
Bits 0 and 3 to 15 cannot be set to 1. |
Dim Stat As Long
SCPI.STATus.QUEStionable.LIMit.ELIMit.NTRansition = 6
Stat = SCPI.STATus.QUEStionable.LIMit.ELIMit.NTRansition
SCPI.STATus.QUEStionable.LIMit.ELIMit.EVENt
SCPI.STATus.QUEStionable.LIMit.ELIMit.PTRansition
No equivalent key is available on the front panel.
:STATus:QUEStionable:LIMit:ELIMit:NTRansition <numeric>
:STATus:QUEStionable:LIMit:ELIMit:NTRansition?
{numeric}<newline><^END>
10 OUTPUT 717;":STAT:QUES:LIM:ELIM:NTR 6"
20 OUTPUT 717;":STAT:QUES:LIM:ELIM:NTR?"
30 ENTER 717;A