SCPI.STATus.QUEStionable.LIMit.NTRansition

Object type

Property (Read-Write)

Syntax

SCPI.STATus.QUEStionable.LIMit.NTRansition = Value

Value = SCPI.STATus.QUEStionable.LIMit.NTRansition

Description

This command sets/gets the value of the negative transition filter of the Questionable Limit Status Register.

Variable

Parameter

Value

Description

Value of the negative transition filter

Data type

Long integer type (Long)

Range

0 to 65535

Preset value

0

Note

The bit 15 can not be set to 1.

Examples

Dim Stat As Long
SCPI.STATus.QUEStionable.LIMit.NTRansition = 6
Stat = SCPI.STATus.QUEStionable.LIMit.NTRansition

Related objects

SCPI.STATus.QUEStionable.LIMit.EVENt

SCPI.STATus.QUEStionable.LIMit.PTRansition

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:STATus:QUEStionable:LIMit:NTRansition <numeric>

:STATus:QUEStionable:LIMit:NTRansition?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":STAT:QUES:LIM:CHAN1:NTR 16"
20 OUTPUT 717;":STAT:QUES:LIM:CHAN1:NTR?"
30 ENTER 717;A