SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.CONDition

Object type    

Property (Read-only)

Syntax         

Value = SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.CONDition

Description

This command reads the value of the Questionable Ripple Limit Channel Extra Status Condition Register of the specified channel.

Variable

Parameter

Value

Description

The value of the Questionable Ripple Limit Channel Extra Status Condition Register.

Data type

Long integer type (Long)

For information on the variable (Ch), see Ch.  

Examples

Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).ECHannel.CONDition

Related objects

SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.NTRansition

SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).ECHannel.PTRansition

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}:ECHannel:CONDition?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":STAT:QUES:RLIM:CHAN1:ECH:COND?"
20 ENTER 717;A