SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).EVENt

Object type    

Property (Read-only)

Syntax         

Value = SCPI.STATus.QUEStionable.RLIMit.CHANnel(Ch).EVENt

Description

This command reads the value of the Questionable Ripple Limit Channel Status Event Register of the specified channel.

Variable

Parameter

Value

Description

The value of the Questionable Ripple Limit Channel Status Event Register.

Data type

Long integer type (Long)

For information on the variable (Ch), see Ch.  

Examples

Dim Stat As Long
Stat = SCPI.STATus.QUEStionable.RLIMit.CHANnel(1).EVENt

Related objects

SCPI.IEEE4882.CLS

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:STATus:QUEStionable:RLIMit:CHANnel{[1]-160}[:EVENt]?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":STAT:QUES:RLIM:CHAN1?"
20 ENTER 717;A