Property (Read-Write)
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.RFON = Param
Param = SCPI.COMMunicate.GPIB.SGENerator.CCOMmand.RFON
This command sets/gets the command to turn on RF for the external signal source in use.
This command is available when the type of the external signal source is 1 (user-defined external signal source).
|
Parameter |
Value |
|
Description |
RF:on setting command for the user-defined external signal source |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Preset value |
"R3" |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
Dim SGcomm As String
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.RFON = "AMPL:STATE ON"
SGcomm = SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.RFON
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.FREQuency
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.POWer
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.CCOMmand.PRESet
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.DWELl
SCPI.SYSTem.COMMunicate.GPIB.SGENerator.TYPE
System > Misc Setup > GPIB Setup > Signal Generator Address > Custom Commands > Turn RF Out On
:SYSTem:COMMunicate:GPIB:SGENerator:CCOMmand:RFON <string>
:SYSTem:COMMunicate:GPIB:SGENerator:CCOMmand:RFON?
{string}<newline><^END>
10 OUTPUT 717;":SYST:COMM:GPIB:SGEN:CCOM:RFON ""AMPL:STATE ON"""
20 OUTPUT 717;":SYST:COMM:GPIB:SGEN:CCOM:RFON?"
30 ENTER 717;A$