Property (Read-only)
Err = SCPI.SYSTem.ERRor
This command reads the oldest error from the list of errors stored in the error queue of the E5072A. The read-out error is deleted from the error queue. The size of the error queue is 100.
Executing SCPI.IEEE4882.CLS command clears the errors stored in the error queue.
This object can not return an error that occurs by the manual operation or the SCPI command used in controlling the E5072A from the external con-troller.
|
Parameter |
Err |
|
Description |
Indicates 2-element array data (for error).
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
|
Note |
If no error is stored in the error queue, 0 and "No error" are read out as the error number and the error message. |
Dim Err As Variant
Err = SCPI.SYSTem.ERRor
No equivalent key is available on the front panel.
:SYSTem:ERRor?
{numeric},{string}<newline><^END>
{numeric}:
Error number
{string}:
Error message (a character string with double quotation marks ("))
If no error is stored in the error queue, 0 and "No error" are read out as the error number and the error message.
10 OUTPUT 717;":SYST:ERR?"
20 ENTER 717;A,B$