Property (Read-only)
Status = SCPI.SYSTem.TEMPerature.STATe
This command does not works in E5072A. This command is provided because of its command compatibility with E5070B/E5071B. On execution, this command does not works and generates no error.
Parameter |
Status |
Description |
Dummy Parameter |
Data type |
Boolean type (Boolean) |
Range |
Always True |
Dim WarmUp As Boolean
WarmUp = SCPI.SYSTem.TEMPerature.STATe
None
:SYSTem:TEMPerature[:STATe]?
{1}<newline><^END>
10 OUTPUT 717;":SYST:TEMP?"
30 ENTER 717;A