Other topics about Analyzing Data
The Fixture Simulator provides the following functions:
Matching Circuit Embedding
Port Impedance Conversion
Network De-embedding
Before you can use any of the features listed above, you must turn ON the desired feature individually and issue the following command to turn ON the Fixture Simulator:
:CALC{1-160}:FSIM:STATThe Matching Circuit feature simulates the characteristics that the DUT would exhibit when connected to a matching circuit.
To turn ON or OFF the Matching Circuit, use the following command:
:CALC{1-160}:FSIM:SEND:PMC:STAT
You can only turn ON or OFF Matching Circuit for all the ports, not for each port individually. However, any port whose circuit type is set to "None" behaves as if this feature is permanently OFF.
To select a circuit type, use the following command:
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}
To set the circuit constant, use the following commands:
|
Circuit constant |
Command |
|
C |
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}:PAR:C |
|
G |
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}:PAR:G |
|
L |
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}:PAR:L |
|
R |
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}:PAR:R |
When you want to use a user file to define the circuit type, specify the file by using the following command:
:CALC{1-160}:FSIM:SEND:PMC:PORT{1-2}:USER:FIL
The Port Impedance Conversion feature converts the measurement results with a port impedance of 50 ohm to the characteristics of a different port impedance.
To turn ON or OFF Port Impedance Conversion, use the following command:
:CALC{1-160}:FSIM:SEND:ZCON:STAT
You can only turn ON or OFF Port Impedance Conversion for all of the ports, not for each port individually. However, any port with ZO set to 50 ohm behaves as if this feature is permanently OFF.
To set the target port impedance, use the following command:
:CALC{1-160}:FSIM:SEND:ZCON:PORT{1-2}:Z0
:CALC{1-160}:FSIM:SEND:ZCON:PORT{1-2}:REAL
:CALC{1-160}:FSIM:SEND:ZCON:PORT{1-2}:IMAG
The Network De-embedding feature eliminates any network that can cause error between the calibration level and the DUT.
To turn ON or OFF Network De-embedding, use the following command:
:CALC{1-160}:FSIM:SEND:DEEM:STAT
You can only turn ON or OFF Network De-embedding for all of the ports, not for each port individually. However, any port whose Network De-embedding type is set to "None" behaves as if this feature is permanently OFF.
To select a Network De-embedding type, use the following command:
:CALC{1-160}:FSIM:SEND:DEEM:PORT{1-2}
To specify the file that defines the criteria for Network De-embedding, use the following command:
:CALC{1-160}:FSIM:SEND:DEEM:PORT{1-2}:USER:FIL
See Fixture Simulator.