Analyzing Impedance

By turning ON the parameter conversion function, you can convert the measurement result of the S-Parameter to the following parameters.

To turn ON/OFF the parameter conversion function, use the following command:

:CALC{1-160}:CONV

To select the parameter to which you want to convert the measurement result, use the following command:

:CALC{1-160}:CONV:FUNC

Other topics about Analyzing Data