LXI

The E5072A is LXI-C compliant.

About LXI

LXI (LAN eXtensions for Instrumentation) is the LAN-based successor to GPIB and combines the advantages of Ethernet with the simplicity and familiarity of GPIB. The key features of LXI are as follows:

Checking LXI Compliance

The E5072A having LXI compliance will show a LXI logo at the start up screen of the firmware . If this logo does not appears at the start up screen of the firmware, it means that the system is not LXI-C complaint.