Power Calibration

Other topics about Performing Calibration

Overview

The E5072A lets you perform power calibration by using a power meter to output a more accurate power level.

Preparation for Power Calibration

Connecting Power Meter and Power Sensor

The E5072A performs power calibration by controlling the power meter via GPIB. Therefore, you need to connect the E5072A and the power meter by using the USB/GPIB interface.

Selecting the Power Meter

Use the following command to select the type of GPIB or USB enabled power meter:

:SYST:COMM:PSENsor

Setting GPIB Address of Power Meter

Use the following command to set the GPIB address of the power meter to the E5072A.

:SYST:COMM:GPIB:PMET:ADDR

Setting Power Sensor Calibration Factor Table

Before performing power calibration, set the reference calibration factor (the calibration factor at 50 MHz) and the calibration factor for each frequency depending on the power sensor you use.

To set the reference calibration factor of the power sensor, use the following commands:

Channel A

:SOUR:POW:PORT:CORR:COLL:ASEN:RCF

Channel B

:SOUR:POW:PORT:CORR:COLL:BSEN:RCF

 

To set the calibration factor table of the power sensor for each frequency, use the following commands:

Channel A

:SOUR:POW:PORT:CORR:COLL:TABL:ASEN:DATA

Channel B

:SOUR:POW:PORT:CORR:COLL:TABL:BSEN:DATA

 

Alternatively, you can configure the power sensor calibration factor table based on the data contained in a CSV file by issuing the following commands:

Channel A

:MMEM:LOAD:ASCF

Channel B

:MMEM:LOAD:BSCF

 

Also, you can save the contents of the current power sensor calibration factor table to a file by issuing the following commands:

Channel A

:MMEM:STOR:ASCF

Channel B

:MMEM:STOR:BSCF

 

For more information on saving/recalling the power sensor calibration factor table, refer to Saving/recalling Power Sensor Calibration Factor Table.

Loss Compensation

You can perform loss compensation by setting in advance the power loss due to the difference in connections (cables, adapters, etc.) between the when the power calibration data are measured and when the actual DUTs are measured.

Setting Loss Compensation Table

To set the loss compensation table for each frequency, use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR:COLL:TABL:LOSS:DATA

Alternatively, you can configure the loss compensation table based on the data contained in a CSV file by issuing the following command:

:MMEM:LOAD:PLOS{1-4}

Also, you can save the contents of the current loss compensation table to a file by issuing the following command:

:MMEM:STOR:PLOS{1-4}

Turning ON/OFF Loss Compensation

To turn on or off the loss compensation, use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR:COLL:TABL:LOSS

Measuring power calibration data

To set the number of power calibration data measurements at one measurement point (averaging factor), use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR:COLL:AVER

To set a tolerance for power calibration, use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR:COLL:NTOL

To measure the power calibration data, use the following command. When the measurement is complete, the power calibration is automatically turned on.

:SOUR{1-36}:POW:PORT{1-4}:CORR:COLL

Turning ON/OFF Power-level Error Correction

To turn on or off the power-level error correction, use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR

When the power calibration data measurement initiated with the :SOUR{1-36}:POW:PORT{1-4}:CORR:COLL command is complete, the power calibration is automatically turned on.

Reading/writing power calibration data array

The power calibration data array contains data used to perform error correction for the power level at each measurement point (values obtained by subtracting the value actually measured with the power meter from the set power level value when measuring power calibration data at each measurement point).

The number of power calibration data arrays that are assigned to individual ports of individual channels can be up to 64 (16x4). To read/write one of the power calibration data arrays, use the following command:

:SOUR{1-36}:POW:PORT{1-4}:CORR:DATA