Managing Files

Other topics about Saving and Recalling

Various Commands

Creating directory (folder)

To create a directory (folder), use the following command:

:MMEM:MDIR

Deleting file (directory)

To delete a file or a directory, use the following command:

:MMEM:DEL

Copying file

To copy a file, use the following command:

:MMEM:COPY

Transferring files

File transfer from the external controller to the E5072A can be possible by reading data from a file on the controller and then writing them to the file on the E5072A.

:MMEM:TRAN

Also, file transfer from the E5072A to the external controller can be possible by reading data from a file on the E5072A using the commands as query and then writing them to the file on the controller.

Retrieving data from storage

To retrieve information for the storage that is built in the E5072A (usage, property of file located in a specified directory), use the following command;

:MMEM:CAT?

Sample Program

See the Transferring Files.