Other topics about Operation Basics
You can save VBA programs either as one complete project or on a module by module basis.
When you opt to save your program as one complete project, you can have the files (modules) making up the project into a single package. A project is saved as a .vba file. You can save your program to a project file using one of the following two methods:
Open the Save As dialog box by doing one of the following:
On the File menu, click Save xxx.VBA. "xxx" represents the file name.
On the toolbar, click Save Project File icon.
Press Ctrl + S keys on the keyboard.
The Save As dialog box appears. Specify the file name and location (drive or folder) and click Save.
Display the E5072A measurement screen following the instructions given in Switching to the E5072A Measurement Screen.
Open the Save As dialog box using the following key sequence:
Macro Setup > Save Project
The Save As dialog box appears. Specify the file name and location (drive or folder) and click Save.
Alternatively, you can save each module (user form, standard, or class) of your VBA program individually. To save a module, you must use Visual Basic Editor. User forms are saved as .frm files, standard modules as .bas files, and class modules as .cls files.
In Project Explorer, click the file name that appears under the desired module icon to highlight it.
Open the Export File dialog box by doing one of the following:
On the File menu, click Export File....
Click the right mouse button, and click Export File....
Press Ctrl + E keys on the keyboard.
The Export File dialog box appears. Specify the file name and location (drive or folder) and click Save.