Other topics about Operation Basics
This section describes how to break a procedure during the execution of a VBA program.
To break the running VBA program, do one of the following:
On the Run menu, click Break.
On the toolbar, click Break Macro icon.
Press Ctrl + Break keys on the keyboard.
Macro Setup > Stop (E5072A measurement screen)
Press Macro Break on the E5072A front panel.
A dialog box is displayed through forced interrupts, and the program is suspended.

Select one of the following:
Continue: Resumes the execution of the program.
End: Terminates the VBA program.
Debug: Displays a run-time error.
Help: Brings up VBA Online Help.
This section describes how to abruptly terminate a running procedure. When abruptly terminating the VBA program by the below methods, the "Program interrupted" message is shown in the instrument status bar on the bottom of the LCD display.
To terminate the running VBA program, do one of the following:
On the Run menu, click Reset.
On the toolbar, click Reset Macro icon.
Insert an End statement into your code.