Value = FirstLeftInterval(Chan)
Returns the stimulus difference between the positive peak detected first when searched from the right edge toward the left edge within the analysis range and its left adjacent negative peak.
FirstLeftInterval
Parameter |
Chan |
Description |
Specifies the channel number. |
Data type |
Integer type (Integer) |
Range |
1 to 9 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
Parameter |
Value |
Description |
Returns the stimulus difference between the positive peak detected first when searched from the right edge toward the left edge within the analysis range and its left adjacent negative peak. |
Data type |
Double precision floating point type (Double) |
Note |
If no applicable point is detected, 0 is returned. |
Dim Value As Double
Value = FirstLeftInterval(1)
MsgBox "First Left Interval =" & Value