Call Pole(Chan,D,LeftStim,LeftValue,RightStim,RightValue)
For the negative peaks below the specified value (D) relative to the maximum value of the positive peaks within the analysis range, returns the response value (LeftValue) and stimulus value (LeftStimulus) of the negative peak first detected when searched to the left from the maximum value of the positive peaks, and the response value (RightValue) and stimulus value (RightStimulus) of the negative peak first detected when searched to the right from the maximum value of the positive peaks.
Pole

|
Parameter |
Chan |
|
Description |
Specifies the channel number. |
|
Data type |
Integer type (Integer) |
|
Range |
1 to 9 |
|
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
|
Parameter |
D |
|
Description |
Specifies the difference from the maximum value. |
|
Data type |
Double precision floating point type (Double) |
|
Parameter |
LeftStim |
|
Description |
Returns the stimulus value of the negative peak first detected to the left from the maximum value of the positive peaks. |
|
Data type |
Double precision floating point type (Double) |
|
Note |
If no applicable point is detected, 0 is returned. |
|
Parameter |
LeftValue |
|
Description |
Returns the response value of the negative peak first detected to the left from the maximum value of the positive peaks. |
|
Data type |
Double precision floating point type (Double) |
|
Note |
If no applicable point is detected, 0 is returned. |
|
Parameter |
RightStim |
|
Description |
Returns the stimulus value of the negative peak first detected to the right from the maximum value of the positive peaks. |
|
Data type |
Double precision floating point type (Double) |
|
Note |
If no applicable point is detected, 0 is returned. |
|
Parameter |
RightValue |
|
Description |
Returns the response value of the negative peak first detected to the right from the maximum value of the positive peaks. |
|
Data type |
Double precision floating point type (Double) |
|
Note |
If no applicable point is detected, 0 is returned. |
Dim LeftStim As Double
Dim LeftValue As Double
Dim RightStim As Double
Dim RightValue As Double
Call Pole(1, 1, LeftStim, LeftValue, RightStim, RightValue)
MsgBox "Left Pole =" & LeftStim & ":" & LeftValue
MsgBox "Right Pole =" & RightStim & ":" & RightValue